This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AH-Q1: mailbox example build problem

Part Number: TDA4AH-Q1

Dear support,

I am using the J784S4XG01EVM eval board and testing different examples from the SDK (ti-processor-sdk-rtos-j784s4-evm-09_00_00_02).

I have gmake and Cygwin tools installed CCS12.4.0.00007_win64 is installed; OpenSSL is installed and the paths are set corrrectly. I am using a Windows 10 PC for building.
Most of the SDK examples I can build e.g. Uart or SPI.

However, when I try to build the mailbox examples I get an error access denied: "make (e=5): Zugriff verweigert", when trying to build:
gmake csl_mailbox_sender_receiver_app BOARD=j784s4_evm CORE=mcu1_1
I copied the build output below. I have tried many things (reboot; build with admin rights; different console, Cygwin,..) but so far I could not fix this problem.

When I try to build for mcu1_0 the build works fine and the binary is generated: (gmake csl_mailbox_sender_receiver_app BOARD=j784s4_evm CORE=mcu1_0).

Best regards
Erwin

--------------------------------------------------------------------------------------------------------------------------------------

/cygdrive/c/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/build


$ gmake csl_mailbox_sender_receiver_app BOARD=j784s4_evm CORE=mcu1_1
gmake -C C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/csl/example/mailbox/mailbox_sender_receiver_app
gmake[1]: Entering directory 'C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/csl/example/mailbox/mailbox_sender_receiver_app'
gmake csl_utils_common csl_uart_console csl uart board udma i2c gpio pm_lib sciclient osal_nonos csl_init
gmake[2]: Entering directory 'C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/csl/example/mailbox/mailbox_sender_receiver_app'
gmake[2]: Nothing to be done for 'csl_utils_common'.
gmake[2]: Nothing to be done for 'csl_uart_console'.
gmake[2]: Nothing to be done for 'csl'.
gmake[2]: Nothing to be done for 'uart'.
gmake[2]: Nothing to be done for 'board'.
gmake[2]: Nothing to be done for 'udma'.
gmake[2]: Nothing to be done for 'i2c'.
gmake[2]: Nothing to be done for 'gpio'.
gmake[2]: Nothing to be done for 'pm_lib'.
gmake[2]: Nothing to be done for 'sciclient'.
gmake[2]: Nothing to be done for 'osal_nonos'.
gmake[2]: Nothing to be done for 'csl_init'.
gmake[2]: Leaving directory 'C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/csl/example/mailbox/mailbox_sender_receiver_app'
gmake C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/binary/csl_mailbox_sender_receiver_app/bin/j784s4_evm/csl_mailbox_sender_receiver_app_mcu1_1_release.xe
r5f
gmake[2]: Entering directory 'C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/csl/example/mailbox/mailbox_sender_receiver_app'
# Compiling j784s4_evm:j784s4:mcu1_1:release:csl_mailbox_sender_receiver_app:mailbox_sender.c
C:/ti/ccs1240/ccs/utils/cygwin/mkdir -p C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/binary/csl_mailbox_sender_receiver_app/obj/j784s4_evm/mcu1_1/release/
C:\ti\ccs1240 /ti-cgt-armllvm_2.1.3.LTS/bin/tiarmclang -MMD -g -DMAKEFILE_BUILD -c -Wall -Werror -Wno-extra -Wno-exceptions -ferror-limit=100 -Wno-unused-command-line-argument -Wno-gnu-variable
-sized-type-not-at-end -Wno-unused-function -Wno-extern-initializer -Wno-excess-initializers -Wno-bitfield-constant-conversion -Wno-address-of-packed-member -fno-strict-aliasing -EL -eo.oer5f -
ea.ser5f -g -mfloat-abi=hard -mfpu=vfpv3-d16 -mcpu=cortex-r5 -march=armv7-r -Werror -flto -Os -s -DBUILD_MCU1_1 -DBUILD_MCU -DBARE_METAL -DSOC_J784S4 -Dj784s4_evm=j784s4_evm -IC:/StgADASDa
ta/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages -IC:\ti\ccs1240 -I/ti-cgt-armllvm_2.1.3.LTS/include/c -c -x c mailbox_sender.c -o C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos
_sdk/pdk_j784s4_09_00_00_45/packages/ti/binary/csl_mailbox_sender_receiver_app/obj/j784s4_evm/mcu1_1/release/mailbox_sender.oer5f -MF C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_
09_00_00_45/packages/ti/binary/csl_mailbox_sender_receiver_app/obj/j784s4_evm/mcu1_1/release/little/.deps/mailbox_sender.d
process_begin: CreateProcess(NULL, C:\ti\ccs1240 /ti-cgt-armllvm_2.1.3.LTS/bin/tiarmclang -MMD -g -DMAKEFILE_BUILD -c -Wall -Werror -Wno-extra -Wno-exceptions -ferror-limit=100 -Wno-unused-comm
and-line-argument -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -Wno-extern-initializer -Wno-excess-initializers -Wno-bitfield-constant-conversion -Wno-address-of-packed-member -
fno-strict-aliasing -EL -eo.oer5f -ea.ser5f -g -mfloat-abi=hard -mfpu=vfpv3-d16 -mcpu=cortex-r5 -march=armv7-r -Werror -flto -Os -s -DBUILD_MCU1_1 -DBUILD_MCU -DBARE_METAL -DSOC_J784S4 -Dj784s4
_evm=j784s4_evm -IC:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages -IC:\ti\ccs1240 -I/ti-cgt-armllvm_2.1.3.LTS/include/c -c -x c mailbox_sender.c -o C:/StgADASDat
a/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/binary/csl_mailbox_sender_receiver_app/obj/j784s4_evm/mcu1_1/release/mailbox_sender.oer5f -MF C:/StgADASData/CIP_CMS3_0/XEg
_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/binary/csl_mailbox_sender_receiver_app/obj/j784s4_evm/mcu1_1/release/little/.deps/mailbox_sender.d, ...) failed.
make (e=5): Zugriff verweigert
gmake[2]: *** [C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/build/makerules/rules_ti_cgt_arm.mk:235: C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j7
84s4_09_00_00_45/packages/ti/binary/csl_mailbox_sender_receiver_app/obj/j784s4_evm/mcu1_1/release/mailbox_sender.oer5f] Error 5
gmake[2]: Leaving directory 'C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/csl/example/mailbox/mailbox_sender_receiver_app'
gmake[1]: *** [C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/build/makerules/common.mk:411: mcu1_1] Error 2
gmake[1]: Leaving directory 'C:/StgADASData/CIP_CMS3_0/XEg_TiEnv/ti_rtos_sdk/pdk_j784s4_09_00_00_45/packages/ti/csl/example/mailbox/mailbox_sender_receiver_app'
gmake: *** [makefile:368: csl_mailbox_sender_receiver_app] Error 2