Part Number: AM62A7
I refer to the EMMC startup process of the am62x chip and find that it does not work
EMMC boot mode steps:
According to the EMMC startup process of the am62x chip, after the execution is complete, switch to EMMC startup mode, and an error is reported in the startup log:
U-Boot SPL 2023.04-g756ba776d4 (Sep 20 2023 - 12:01:11 +0800) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') am62a_init: board_init_f done SPL initial stack usage: 17032 bytes am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0 Trying to boot from MMC1 mmc_load_image_raw_sector: mmc block read error ** Partition 1 not valid on device 0 ** spl_register_fat_device: fat register err - -1 spl_load_image_fat: error reading image tispl.bin, err - -1 SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###
SD card boot log:
U-Boot SPL 2023.04-g756ba776d4 (Sep 20 2023 - 12:01:11 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
am62a_init: board_init_f done
SPL initial stack usage: 17032 bytes
am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0
Trying to boot from MMC2
am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0
Authentication passed
am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0
Authentication passed
am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0
Authentication passed
am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0
Authentication passed
am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0
Authentication passed
Starting ATF on ARM64 core...
NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 00:42:57, Jan 13 2023
U-Boot SPL 2023.04-g756ba776d4 (Sep 20 2023 - 12:00:33 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
am62a_init: board_init_f done
am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0
Trying to boot from MMC2
am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0
Authentication passed
am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0
Authentication passed
U-Boot 2023.04-g756ba776d4 (Sep 20 2023 - 12:00:33 +0800)
SoC: AM62AX SR1.0 HS-FS
Model: Texas Instruments AM62A7 SK
DRAM: 1 GiB
Core: 57 devices, 27 uclasses, devicetree: separate
MMC: mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Net: Could not get PHY for ethernet@8000000port@1: addr 0
am65_cpsw_nuss_port ethernet@8000000port@1: phy_connect() failed
No ethernet found.
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
ERROR: reserving fdt memory region failed (addr=ae000000 size=12000000 flags=4)
669 bytes read in 26 ms (24.4 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
## Error: "main_cpsw0_qsgmii_phyinit" not defined
ERROR: reserving fdt memory region failed (addr=ae000000 size=12000000 flags=4)
20593152 bytes read in 881 ms (22.3 MiB/s)
ERROR: reserving fdt memory region failed (addr=ae000000 size=12000000 flags=4)
53586 bytes read in 31 ms (1.6 MiB/s)
Working FDT set to 88000000
ERROR: reserving fdt memory region failed (addr=ae000000 size=12000000 flags=4)
2149 bytes read in 27 ms (77.1 KiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
Loading Device Tree to 000000008feef000, end 000000008fffffff ... OK
Working FDT set to 8feef000
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 6.1.33-00003-g6a5933cb38aa-dirty (cnh20399@cnh20399-Latitude-7390-2-in-1) (aarch64-none-linux-gnu-gcc (Arm GNU Toolchain 11.3.Rel1) 11.3.1 20220712, GNU ld (Arm GNU Toolchain 11.3.Rel1) 2.38.20220708) #9 SMP PREEMPT Sat Oct 7 15:51:03 CST 2023
[ 0.000000] Machine model: Texas Instruments AM62A7 SK
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: failed to allocate memory for node 'linux,cma': size 576 MiB
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000099800000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node c7x-dma-memory@99800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000099900000, size 30 MiB
[ 0.000000] OF: reserved mem: initialized node c7x-memory@99900000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009b800000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009b900000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b900000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c900000, size 30 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c900000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 32 MiB
[ 0.000000] OF: reserved mem: initialized node edgeai-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: initialized node edgeai_shared-memories, compatible id dma-heap-carveout
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ae000000, size 288 MiB
[ 0.000000] OF: reserved mem: initialized node edgeai-core-heap-memory@ae000000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000997fffff]
[ 0.000000] node 0: [mem 0x0000000099800000-0x000000009b7fefff]
[ 0.000000] node 0: [mem 0x000000009b800000-0x000000009e6fffff]
[ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff]
[ 0.000000] node 0: [mem 0x000000009e780000-0x00000000a2ffffff]
[ 0.000000] node 0: [mem 0x00000000a3000000-0x00000000adffffff]
[ 0.000000] node 0: [mem 0x00000000ae000000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] On node 0, zone DMA: 1 pages in unavailable ranges
[ 0.000000] cma: Reserved 32 MiB at 0x0000000096600000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 19 pages/cpu s38376 r8192 d31256 u77824
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 258047
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=e0c72754-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 345144K/1048572K available (12480K kernel code, 1294K rwdata, 4048K rodata, 2176K init, 498K bss, 670660K reserved, 32768K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 256 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000080040000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080050000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008489] Console: colour dummy device 80x25
[ 0.013071] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023752] pid_max: default: 32768 minimum: 301
[ 0.028521] LSM: Security Framework initializing
[ 0.033330] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.040901] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.050375] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.057815] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.064103] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.070478] rcu: Hierarchical SRCU implementation.
[ 0.075383] rcu: Max phase no-delay instances is 1000.
[ 0.080932] Platform MSI: msi-controller@1820000 domain created
[ 0.087188] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.097004] EFI services will not be available.
[ 0.101879] smp: Bringing up secondary CPUs ...
[ 0.107147] Detected VIPT I-cache on CPU1
[ 0.107233] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[ 0.107250] GICv3: CPU1: using allocated LPI pending table @0x0000000080060000
[ 0.107297] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.107951] Detected VIPT I-cache on CPU2
[ 0.108014] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[ 0.108028] GICv3: CPU2: using allocated LPI pending table @0x0000000080070000
[ 0.108059] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.108650] Detected VIPT I-cache on CPU3
[ 0.108708] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[ 0.108722] GICv3: CPU3: using allocated LPI pending table @0x0000000080080000
[ 0.108750] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.108808] smp: Brought up 1 node, 4 CPUs
[ 0.188526] SMP: Total of 4 processors activated.
[ 0.193338] CPU features: detected: 32-bit EL0 Support
[ 0.198608] CPU features: detected: CRC32 instructions
[ 0.203919] CPU: All CPU(s) started at EL2
[ 0.208116] alternatives: applying system-wide alternatives
[ 0.215090] devtmpfs: initialized
[ 0.225677] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.235687] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.243641] pinctrl core: initialized pinctrl subsystem
[ 0.249537] DMI not present or invalid.
[ 0.254023] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.260993] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[ 0.268418] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.276436] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.284598] audit: initializing netlink subsys (disabled)
[ 0.290249] audit: type=2000 audit(0.184:1): state=initialized audit_enabled=0 res=1
[ 0.290672] thermal_sys: Registered thermal governor 'step_wise'
[ 0.298180] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.304358] cpuidle: using governor menu
[ 0.315191] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.322211] ASID allocator initialised with 65536 entries
[ 0.339326] KASLR disabled due to lack of seed
[ 0.350581] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.357546] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.363956] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.370896] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.377304] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.384243] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.390650] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.397589] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.405410] k3-chipinfo 43000014.chipid: Family:AM62AX rev:SR1.0 JTAGID[0x0bb8d02f] Detected
[ 0.415502] iommu: Default domain type: Translated
[ 0.420511] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.427182] SCSI subsystem initialized
[ 0.431334] usbcore: registered new interface driver usbfs
[ 0.436978] usbcore: registered new interface driver hub
[ 0.442430] usbcore: registered new device driver usb
[ 0.448028] pps_core: LinuxPPS API ver. 1 registered
[ 0.453106] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.462462] PTP clock support registered
[ 0.466580] EDAC MC: Ver: 3.0.0
[ 0.470518] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fca100
[ 0.477338] omap-mailbox 29010000.mailbox: omap mailbox rev 0x66fca100
[ 0.484136] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fca100
[ 0.490866] omap-mailbox 29030000.mailbox: no available mbox devices found
[ 0.498281] FPGA manager framework
[ 0.501827] Advanced Linux Sound Architecture Driver Initialized.
[ 0.508899] clocksource: Switched to clocksource arch_sys_counter
[ 0.515352] VFS: Disk quotas dquot_6.6.0
[ 0.519400] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.532106] Carveout Heap: Exported 176 MiB at 0x00000000a3000000
[ 0.538456] NET: Registered PF_INET protocol family
[ 0.543567] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.552109] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
[ 0.560718] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.568653] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.576630] TCP bind hash table entries: 8192 (order: 6, 262144 bytes, linear)
[ 0.584226] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.590822] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.597616] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.604986] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.611137] RPC: Registered named UNIX socket transport module.
[ 0.617211] RPC: Registered udp transport module.
[ 0.622020] RPC: Registered tcp transport module.
[ 0.626829] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.633417] NET: Registered PF_XDP protocol family
[ 0.638326] PCI: CLS 0 bytes, default 64
[ 0.642959] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.652721] Initialise system trusted keyrings
[ 0.657482] workingset: timestamp_bits=46 max_order=17 bucket_order=0
[ 0.669589] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.676171] NFS: Registering the id_resolver key type
[ 0.681388] Key type id_resolver registered
[ 0.685667] Key type id_legacy registered
[ 0.689827] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.696683] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.704417] 9p: Installing v9fs 9p2000 file system support
[ 0.745124] Key type asymmetric registered
[ 0.749314] Asymmetric key parser 'x509' registered
[ 0.754343] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.762053] io scheduler mq-deadline registered
[ 0.766693] io scheduler kyber registered
[ 0.773564] pinctrl-single 4084000.pinctrl: 34 pins, size 136
[ 0.779854] pinctrl-single f4000.pinctrl: 171 pins, size 684
[ 0.792288] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.805949] loop: module loaded
[ 0.810412] megasas: 07.719.03.00-rc1
[ 0.817800] tun: Universal TUN/TAP device driver, 1.6
[ 0.823600] thunder_xcv, ver 1.0
[ 0.826938] thunder_bgx, ver 1.0
[ 0.830265] nicpf, ver 1.0
[ 0.833383] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 0.840771] hns3: Copyright (c) 2017 Huawei Corporation.
[ 0.846259] hclge is initializing
[ 0.849665] e1000: Intel(R) PRO/1000 Network Driver
[ 0.854650] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 0.860554] e1000e: Intel(R) PRO/1000 Network Driver
[ 0.865628] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 0.871707] igb: Intel(R) Gigabit Ethernet Network Driver
[ 0.877226] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 0.882946] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.889353] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.895517] sky2: driver version 1.30
[ 0.899858] VFIO - User Level meta-driver version: 0.3
[ 0.905727] usbcore: registered new interface driver usb-storage
[ 0.912523] i2c_dev: i2c /dev entries driver
[ 0.918847] sdhci: Secure Digital Host Controller Interface driver
[ 0.925217] sdhci: Copyright(c) Pierre Ossman
[ 0.930084] Synopsys Designware Multimedia Card Interface Driver
[ 0.936608] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.943165] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.949477] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.956383] usbcore: registered new interface driver usbhid
[ 0.962088] usbhid: USB HID core driver
[ 0.967116] optee: probing for conduit method.
[ 0.971714] optee: revision 3.20 (8e74d476)
[ 0.971980] optee: dynamic shared memory is enabled
[ 0.981601] optee: initialized driver
[ 0.986758] Initializing XFRM netlink socket
[ 0.991173] NET: Registered PF_PACKET protocol family
[ 0.996454] 9pnet: Installing 9P2000 support
[ 1.000878] Key type dns_resolver registered
[ 1.005596] registered taskstats version 1
[ 1.009817] Loading compiled-in X.509 certificates
[ 1.021993] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
[ 1.065291] i2c 0-0010: Fixed dependency cycle(s) with /bus@f0000/ticsi2rx@30102000/csi-bridge@30101000
[ 1.075482] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[ 1.082333] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
[ 1.088746] omap_i2c 20020000.i2c: bus 2 rev0.12 at 400 kHz
[ 1.094685] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
[ 1.103026] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
[ 1.112255] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[ 1.121346] ti-sci-inta 4e0a0000.interrupt-controller: Interrupt Aggregator domain 200 created
[ 1.131057] ti-udma 485c0100.dma-controller: Number of rings: 82
[ 1.139119] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
[ 1.150001] ti-udma 485c0000.dma-controller: Number of rings: 150
[ 1.160073] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
[ 1.169439] ti-udma 4e230000.dma-controller: Number of rings: 6
[ 1.175945] ti-udma 4e230000.dma-controller: Channels: 6 (bchan: 0, tchan: 0, rchan: 6)
[ 1.185259] printk: console [ttyS2] disabled
[ 1.189690] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 252, base_baud = 3000000) is a 8250
[ 1.198570] printk: console [ttyS2] enabled
[ 1.198570] printk: console [ttyS2] enabled
[ 1.207025] printk: bootconsole [ns16550a0] disabled
[ 1.207025] printk: bootconsole [ns16550a0] disabled
[ 1.619300] spi-nand: probe of spi0.0 failed with error -110
[ 1.625506] k3-j72xx-soc-thermal b00000.temperature-sensor: invalid resource
[ 1.632588] k3-j72xx-soc-thermal: probe of b00000.temperature-sensor failed with error -22
[ 1.644038] mmc1: CQHCI version 5.10
[ 1.644173] mmc0: CQHCI version 5.10
[ 1.688966] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[ 1.696503] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[ 1.741530] mmc1: new high speed SDHC card at address aaaa
[ 1.747595] mmcblk1: mmc1:aaaa SD32G 29.7 GiB
[ 1.754057] mmcblk1: p1 p2
[ 1.900010] mmc0: Command Queue Engine enabled
[ 1.904508] mmc0: new HS200 MMC card at address 0001
[ 1.910357] mmcblk0: mmc0:0001 8GUF4R 7.28 GiB
[ 1.916119] mmcblk0: p1
[ 1.919107] mmcblk0boot0: mmc0:0001 8GUF4R 31.9 MiB
[ 1.924867] mmcblk0boot1: mmc0:0001 8GUF4R 31.9 MiB
[ 1.930556] mmcblk0rpmb: mmc0:0001 8GUF4R 4.00 MiB, chardev (240:0)
[ 2.007157] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 2.015495] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 2.022925] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 2.038614] ALSA device list:
[ 2.041618] No soundcards found.
[ 2.563802] EXT4-fs (mmcblk1p2): recovery complete
[ 2.569696] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
[ 2.578311] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.587556] devtmpfs: mounted
[ 2.591392] Freeing unused kernel memory: 2176K
[ 2.596038] Run /sbin/init as init process
[ 3.049354] systemd[1]: System time before build time, advancing clock.
[ 3.186306] NET: Registered PF_INET6 protocol family
[ 3.193126] Segment Routing with IPv6
[ 3.196832] In-situ OAM (IOAM) with IPv6
[ 3.245843] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[ 3.278378] systemd[1]: Detected architecture arm64.
Welcome to Arago 2023.04!
[ 3.363299] systemd[1]: Hostname set to <am62axx-evm>.
[ 3.504347] systemd-sysv-generator[150]: SysV service '/etc/init.d/halt' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.530604] systemd-sysv-generator[150]: SysV service '/etc/init.d/netopeer2-server' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.555713] systemd-sysv-generator[150]: SysV service '/etc/init.d/sysrepo' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.579804] systemd-sysv-generator[150]: SysV service '/etc/init.d/umountnfs.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.604149] systemd-sysv-generator[150]: SysV service '/etc/init.d/single' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.627945] systemd-sysv-generator[150]: SysV service '/etc/init.d/psplash.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.652267] systemd-sysv-generator[150]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.678365] systemd-sysv-generator[150]: SysV service '/etc/init.d/sendsigs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.704130] systemd-sysv-generator[150]: SysV service '/etc/init.d/telnetd' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.728510] systemd-sysv-generator[150]: SysV service '/etc/init.d/reboot' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.752253] systemd-sysv-generator[150]: SysV service '/etc/init.d/save-rtc.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.779274] systemd-sysv-generator[150]: SysV service '/etc/init.d/docker.init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.805468] systemd-sysv-generator[150]: SysV service '/etc/init.d/umountfs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.829863] systemd-sysv-generator[150]: SysV service '/etc/init.d/netperf' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.853732] systemd-sysv-generator[150]: SysV service '/etc/init.d/inetd.busybox' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.878070] systemd-sysv-generator[150]: SysV service '/etc/init.d/dropbear' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.902712] systemd-sysv-generator[150]: SysV service '/etc/init.d/edgeai-launcher.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.318370] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[ 4.387950] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[ 4.468587] systemd[1]: Queued start job for default target Graphical Interface.
[ 4.532538] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 4.555834] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 4.580278] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 4.604805] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 4.623722] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password ��ts to Console Directory Watch.
[ 4.649383] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R��uests to Wall Directory Watch.
[ 4.673735] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 4.689253] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 4.709271] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 4.725225] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 4.793827] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 4.817421] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 4.858481] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 4.881906] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 4.908590] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 4.931579] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.955678] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.976727] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 5.004217] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 5.027211] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 5.051585] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 5.117604] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 5.140880] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 5.193511] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 5.210264] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[ 5.235875] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 5.261740] systemd[1]: Starting Create List of Static Device Nodes...
Starting Create List of Static Device Nodes...
[ 5.313838] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 5.339356] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 5.362529] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 5.407368] fuse: init (API version 7.37)
[ 5.442148] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 5.480621] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 5.497389] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
[ 5.519177] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 5.542353] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 5.563016] systemd[1]: Starting Generate network units from Kernel command line...
Starting Generate network ��ts from Kernel command line...
[ 5.590552] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 5.611175] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
[ 5.661748] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 5.689768] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 5.705931] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Create List of Static Device Nodes.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star��progress communication helper.
[ OK ] Finished Load Kernel Modules.
[ OK ] Finished Generate network units from Kernel command line.
[ OK ] Finished Remount Root and Kernel File Systems.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 6.107537] systemd-journald[165]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /media/ram...
Mounting /var/volatile...
[ 6.352760] audit: type=1334 audit(1651167748.304:2): prog-id=5 op=LOAD
[ 6.359589] audit: type=1334 audit(1651167748.312:3): prog-id=6 op=LOAD
Starting Rule-based Manage��for Device Events and Files...
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Rule-based Manager for Device Events and Files.
[ OK ] Finished Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ 6.970990] random: crng init done
[ OK ] Started Network Time Synchronization.
[ OK ] Finished Load/Save Random Seed.
[ 7.026791] mc: Linux media interface: v0.10
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.[ 7.070378] videodev: Linux video capture interface: v2.00
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timer Units.
[ 7.110792] === ar0144_probe
[ 7.114032] === ar0144_check_hwcfg
[ 7.118984] === ar0144_power_on
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ 7.129685] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
[ OK ] Listening on D-Bus System Message B[ 7.143025] vdec 30210000.video-codec: error -ENXIO: IRQ index 0 not found
us Socket.
[ 7.155796] vdec 30210000.video-codec: failed to get irq resource, falling back to polling
[ 7.155862] k3-dsp-rproc 7e000000.dsp: assigned reserved memory node c7x-dma-memory@99800000
[ 7.174176] platform 79000000.r5f: configured R5F for remoteproc mode
[ 7.180680] k3-dsp-rproc 7e000000.dsp: configured DSP for remoteproc mode
[ 7.184957] === ar0144_power_on max96714 is locked, loops:1
[ 7.185063] remoteproc remoteproc0: 7e000000.dsp is available
[ 7.188254] platform 79000000.r5f: assigned reserved memory node r5f-dma-memory@9b800000
[ 7.193231] === ar0144_identify_module,
[ 7.193244] === ar0144_read_reg, i2c_addr = 0x28 reg = 0xd, len = 0x1
Starting Docker Socket for the API...
[ 7.217935] === ar0144_read_reg, i2c_addr = 0x28 reg = 0xd, len = 0x1, read_data = 0xca
[ 7.227507] remoteproc remoteproc1: 79000000.r5f is available
[ 7.231611] === ar0144_init_controls
[ 7.239674] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[ 7.240782] === ar0144_set_default_format w:1280, h:800, code:0x0, colorspace:0x0, field:0x0
[ 7.252766] platform 78000000.r5f: configured R5F for IPC-only mode
[ 7.262222] === ar0144_power_off
[ 7.267687] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9c800000
[ 7.287652] remoteproc remoteproc2: 78000000.r5f is available
[ 7.293559] remoteproc remoteproc2: attaching to 78000000.r5f
[ 7.299979] platform 78000000.r5f: R5F core initialized in IPC-only mode
[ 7.306774] rproc-virtio rproc-virtio.5.auto: assigned reserved memory node r5f-dma-memory@9c800000
[ 7.316500] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 7.317161] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd
[ 7.322088] rproc-virtio rproc-virtio.5.auto: registered virtio0 (type 7)
[ 7.334029] remoteproc remoteproc1: powering up 79000000.r5f
[ 7.335897] remoteproc remoteproc2: remote processor 78000000.r5f is now attached
[ 7.341579] remoteproc remoteproc1: Booting fw image am62a-mcu-r5f0_0-fw, size 523192
[ 7.358159] remoteproc remoteproc1: bad phdr da 0x9c900000 mem 0x8c
[ 7.364651] remoteproc remoteproc1: Failed to load program segments: -22
[ OK ] Listening on dropbear.socket.
Starting Weston socket...
Starting Console System Startup Logging...
Starting D-Bus System Message Bus...
Starting Reboot and dump vmcore via kexec.[ 7.524178] e5010 fd20000.e5010: Device registered as /dev/video2
..
[ OK ] Listening on Docker Socket for the API.
[ OK ] Listening on Weston socket.
[ OK ] Found device /dev/ttyS2.
[ OK ] Reached target Socket Units.
[ 7.647136] remoteproc remoteproc0: powering up 7e000000.dsp
[ 7.652932] remoteproc remoteproc0: Booting fw image am62a-c71_0-fw, size 6897744
[ 7.668214] k3-dsp-rproc 7e000000.dsp: booting DSP core using boot addr = 0x99a00000
[ 7.691758] rproc-virtio rproc-virtio.6.auto: assigned reserved memory node c7x-dma-memory@99800000
[ 7.708327] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 7.709672] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xd
[ 7.714125] rproc-virtio rproc-virtio.6.auto: registered virtio1 (type 7)
[ 7.721244] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x15
[ 7.727837] remoteproc remoteproc0: remote processor 7e000000.dsp is now up
[ 7.742224] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xe
[ 7.749954] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0x15
[ 7.757386] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xe
[ OK ] Finished Console System Startup Logging.
[ OK ] Finished Reboot and dump vmcore via kexec.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting Telephony service...
Starting Expand the rootfs��ll size of the boot device....
[ 8.066838] audit: type=1334 audit(1651275233.308:4): prog-id=7 op=LOAD
[ 8.073641] audit: type=1334 audit(1651275233.316:5): prog-id=8 op=LOAD
Starting User Login Management...
[ OK ] Started TEE Supplicant.
Starting telnetd.service...
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Reached target Preparation for Network.
Starting Network Configuration...
[ OK ] Started telnetd.service.
[ OK ] Started Telephony service.
[ 8.588691] ar0144 0-0010: Consider updating driver ar0144 to match on endpoints
[ 8.598326] cdns-csi2rx 30101000.csi-bridge: Probed CSI2RX with 4/4 lanes, 4 streams, external D-PHY
[ 8.604018] ================= [ar0144 0-0010-subdev_do_ioctl] cmd:0x80685600 =================
[ 8.647090] ================= [30102000.ticsi2rx-subdev_do_ioctl] cmd:0x80685600 =================
[ 8.648543] ================= [cdns_csi2rx.30101000.csi-bridge-subdev_do_ioctl] cmd:0x80685600 =================
[ 8.724121] xhci-hcd xhci-hcd.7.auto: xHCI Host Controller
[ 8.731400] xhci-hcd xhci-hcd.7.auto: new USB bus registered, assigned bus number 1
[ 8.739409] xhci-hcd xhci-hcd.7.auto: USB3 root hub has no ports
[ 8.739427] xhci-hcd xhci-hcd.7.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010
[ 8.739592] xhci-hcd xhci-hcd.7.auto: irq 538, io mem 0x31100000
[ 8.744136] hub 1-0:1.0: USB hub found
[ OK ] Listening on Load/Save RF ��itch S[ 8.768327] hub 1-0:1.0: 1 port detected
tatus /dev/rfkill Watch.
[ 8.769361] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 8.797941] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 8.825929] Bluetooth: Core ver 2.22
[ 8.829721] NET: Registered PF_BLUETOOTH protocol family
[ 8.835100] Bluetooth: HCI device and connection manager initialized
[ 8.841529] Bluetooth: HCI socket layer initialized
[ 8.846493] Bluetooth: L2CAP socket layer initialized
[ 8.846544] Bluetooth: SCO socket layer initialized
[ OK ] Finished Expand the rootfs��full size of the boot device..
[ OK ] Started Network Configuration.
Starting Wait for Network to be Configured...
Starting Network Name Resolution...
[ OK ] Created slice Slice /system/systemd-fsck.
[ OK ] Found device /dev/mmcblk0p1.
Starting File System Check on /dev/mmcblk0p1...
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting Avahi mDNS/DNS-SD Stack...
Starting Enable and configure wl18xx bluetooth stack...
Starting containerd container runtime...
[ OK ] Started Netperf Benchmark Server.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Permit User Sessions...
[ OK ] Finished Enable and configure wl18xx bluetooth stack.
[ OK ] Finished Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
Starting Weston, a Wayland��ositor, as a system service...
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Finished File System Check on /dev/mmcblk0p1.
Mounting /run/media/mmcblk0p1...
[ OK ] Found device /dev/mmcblk1p1.
[ 9.855529] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Quota mode: none.
Starting File System Check on /dev/mmcblk1p1...
[ OK ] Mounted /run/media/mmcblk0p1.
[ 10.129739] audit: type=1334 audit(1651275235.372:6): prog-id=9 op=LOAD
[ 10.136636] audit: type=1334 audit(1651275235.376:7): prog-id=10 op=LOAD
Starting User Database Manager...
[ OK ] Started User Database Manager.
[ OK ] Created slice User Slice of UID 1000.
Starting User Runtime Directory /run/user/1000...
[ OK ] Finished File System Check on /dev/mmcblk1p1.
[ OK ] Finished User Runtime Directory /run/user/1000.
Mounting /run/media/BOOT-mmcblk1p1...
Starting User Manager for UID 1000...
[ 10.894633] audit: type=1006 audit(1651275236.136:8): pid=563 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
[ 10.907354] audit: type=1300 audit(1651275236.136:8): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffc2c98f98 a2=4 a3=ffff89629020 items=0 ppid=1 pid=563 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[ 10.933986] audit: type=1327 audit(1651275236.136:8): proctitle="(systemd)"
[ OK ] Mounted /run/media/BOOT-mmcblk1p1.
[ OK ] Started User Manager for UID 1000.
[ OK ] Started Session c1 of User weston.
[ 11.666311] audit: type=1006 audit(1651275236.908:9): pid=519 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=2 res=1
[ 11.678797] audit: type=1300 audit(1651275236.908:9): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffc2c98f98 a2=4 a3=ffff89629020 items=0 ppid=1 pid=519 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
[ 11.710095] audit: type=1327 audit(1651275236.908:9): proctitle="(weston)"
[FAILED] Failed to start Weston, a ��mpositor, as a system service.
See 'systemctl status weston.service' for details.
Starting EdgeAI OOB demos...
[ OK ] Started containerd container runtime.
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
adwaita-icon-theme-symbolic
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
g++-symlinks
g++
gawk-dev
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gnu-config
grub-common
grub-editenv
grub-efi
gzip
less
libasm1
libatomic-dev
libatomic1
libbfd
libdebuginfod1
libdw1
libeigen-dev
libelf1
libgcc-s-dev
libgcc1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp10
libidn2-0
libmpc3
libmpfr6
libopcodes
libqt5charts-examples
libqt5charts-plugins
libqt5charts-qmlplugins
libqt5charts5
libqt5sensors-plugins
libqt5sensors-qmlplugins
libqt5sensors5
libqt5serialport-examples
libqt5serialport-plugins
libqt5serialport-qmlplugins
libqt5serialport5
libqt5svg-examples
libqt5svg-plugins
libqt5svg-qmlplugins
libqt5svg5
libqt5virtualkeyboard-plugins
libqt5virtualkeyboard-qmlplugins
libqt5virtualkeyboard5
libqt5webchannel-plugins
libqt5webchannel-qmlplugins
libqt5webchannel5
libreadline-dev
libreadline8
libstdc++-dev
libstdc++6
libunistring2
m4-dev
m4
make
nettle
parted
piglit
qt3d-plugins
qt3d-qmlplugins
qt3d
qtbase-examples
qtbase-plugins
qtbase-qmlplugins
qtbase
qtconnectivity-plugins
qtconnectivity-qmlplugins
qtconnectivity
qtdeclarative-plugins
qtdeclarative-qmlplugins
qtdeclarative-tools
qtdeclarative
qtgraphicaleffects-qmlplugins
qtlocation-examples
qtlocation-plugins
qtlocation-qmlplugins
qtlocation
qtmultimedia-examples
qtmultimedia-plugins
qtmultimedia-qmlplugins
qtmultimedia
qtquick3d-plugins
qtquick3d-qmlplugins
qtquick3d
qtquics-qmlplugins.control
qtquics2-plugins.control
qtquics2-qmlplugins.control
qtquics2.control
qtscript-examples
qtscript-plugins
qtscript-qmlplugins
qtscript
qtwayland-examples
qtwayland-plugins
qtwayland-qmlplugins
qtwayland
tar
which
If you do not wish to distribute GPL-3.0 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project am62axx-evm -
Arago 2023.04 am62axx-evm -
am62axx-evm login: root
[ 19.149008] audit: type=1006 audit(1651275244.388:10): pid=1059 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=3 res=1
[ 19.161684] audit: type=1300 audit(1651275244.388:10): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffc2c98f98 a2=1 a3=ffff89629020 items=0 ppid=1 pid=1059 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[ 19.188187] audit: type=1327 audit(1651275244.388:10): proctitle="(systemd)"
[ 19.195326] audit: type=1334 audit(1651275244.416:11): prog-id=11 op=LOAD
[ 19.202188] audit: type=1300 audit(1651275244.416:11): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffd2abfef0 a2=78 a3=0 items=0 ppid=1 pid=1059 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
[ 19.227725] audit: type=1327 audit(1651275244.416:11): proctitle="(systemd)"
[ 19.234901] audit: type=1334 audit(1651275244.428:12): prog-id=11 op=UNLOAD
[ 19.241942] audit: type=1334 audit(1651275244.428:13): prog-id=12 op=LOAD
[ 19.248830] audit: type=1300 audit(1651275244.428:13): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffd2abff90 a2=78 a3=0 items=0 ppid=1 pid=1059 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
[ 19.274343] audit: type=1327 audit(1651275244.428:13): proctitle="(systemd)"
-sh: ./init_script.sh: No such file or directory
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps# df -h
Filesystem Size Used Avail Use% Mounted on
/dev/root 29G 5.7G 22G 21% /
devtmpfs 169M 4.0K 169M 1% /dev
tmpfs 186M 0 186M 0% /dev/shm
tmpfs 75M 8.9M 66M 12% /run
tmpfs 4.0M 0 4.0M 0% /sys/fs/cgroup
tmpfs 186M 8.0K 186M 1% /tmp
tmpfs 16M 0 16M 0% /media/ram
tmpfs 50M 12K 50M 1% /var/volatile
/dev/mmcblk0p1 7.1G 7.1G 0 100% /run/media/mmcblk0p1
tmpfs 38M 0 38M 0% /run/user/1000
/dev/mmcblk1p1 124M 2.9M 122M 3% /run/media/BOOT-mmcblk1p1
tmpfs 38M 0 38M 0% /run/user/0
root@am62axx-evm:/opt/edgeai-gst-apps#