Other Parts Discussed in Thread: AM1802, OMAP-L138, AM1808
What steps do I need to take to setup a custom AM180x based board for the first time? Can I use JTAG to install u-boot? Do I need to use one of the boot modes of the AM180x to install u-boot? Is there a document that shows the workflow of setting up a board for the first time?
I am using Virtual box on Windows 7. I have a Ubuntu 10.10.16G installation as my linux host. I have a Blackhawk USB100v2 JTAG dongle. I have a custom board with a AM1802 processor with NAND flash and mDDR ram.
Linux appears to load the drivers for the USB100v2 and I set it up in CCS with a target configuration. However, I've found no documentation that describes where to go from there. How do I take the u-boot binary file and flash it to the board?
Thanks,
David