This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VE-Q1: TDA4 APA Ultrasonic Radar Driver Pinout Confirmation

Part Number: TDA4VE-Q1
Other Parts Discussed in Thread: SYSCONFIG

Hi,TI's firend:

APA PROJECT; could you verify that the following pins are reasonable?

NO. TDA4 EPWM  OUTPUT  PWM
1 U28 EHRPWM0_A
2 W28 EHRPWM0_B
3 AC27 EHRPWM1_A
4 R28 EHRPWM1_B
5 AC28 EHRPWM2_A
6 U27 EHRPWM2_B
7 T25 EHRPWM3_A
8 T24 EHRPWM3_B
9 T23 EHRPWM4_A
10 Y25 EHRPWM4_B
11 AA28 EHRPWM4_A
12 U26 EHRPWM4_B
NO. TDA4 GPIO+DMA CAPTURE PWM
1 V27 GPIO19
2 W27 GPIO20
3 Y27 GPIO21
4 AA27 GPIO22
5 AA26 GPIO23
6 T27 GPIO31
7 W24 GPIO36
8 AA25 GPIO37
9 V25 GPIO38
10 AB25 GPIO40
11 U24 GPIO42
12 AC25 GPIO43