This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62B: Splash logo on AM62 , uboot / kernel?

Part Number: SK-AM62B

https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_00_00_03/exports/docs/linux/Foundational_Components/U-Boot/UG-Splash-Screen.html?highlight=splash

Champs:

Customer needs to show their logo in some seconds (~ 5 Seconds).

#1.

According the above link, the early splash should appear in the uboot stage.

However, the must-have requirement is the uboot shall have the LVDS working.

But how?

   Any patch for uboot LVDS enabled the LCD?

#2.

Despite the uboot splash, customer is checking if they can force the kernel to show the log.

Is it possible to force this API for showing the log?

in this file: board-support/ti-linux-kernel/drivers/video/fbdev/core/fbcon.c  

in this api: fbcon_prepare_logo

please comment for each.

Thanks.

BR Rio

BR Rio