Other Parts Discussed in Thread: TMS320DM365
Hello,
I have taken over a design that uses the TMS320DM365 device. Currently, The AEMIF interface is only connected to an on-board NAND Flash using an 8-bit bus.
Previous designer states that 16-bit bus is provided in the main interface connector of this design for future development (EM_CE1).
Although the AECFG[2:0] lines are available to be configured for either 8-bit or 16-bit bus, terminal EM_BA1/GIO66/KEYB1/HINTN (bga ID R17) in not provided.
I assume this is a problem when trying to address 16-bit memory devices. Am I correct or I'm missing something?
Regards and thank you for your feedback.
Elvis Mota