This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM263: Detect device and run example

Part Number: LP-AM263


Hi,

I use a TI Launchpad AM263x board and try to run an example with code composer.

I did the fully installation of code composer and download MCU PLUS SDK and Motor Control SDK.

I can't use any project example with the board, when I check the device with the target configuration I have an error message :

Same error with AM263x board. The device appears in window control panel with name "XDS110", device is plugged with micro USB and USB-C connector.

Any idea about this issue ?