This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR2 configuration for C6472 and MT47H128M16HG-3

(posted this by accident in the single-core DSP forum - same post)

Hi -

We're trying to bring up a board here using 2 of these DDR2 chips (recommended under TI guidelines), and are having problems. Since it's a new board, we can't tell whether there are issues with the board itself or whether our timing values are simply wrong. I'd like to eliminate the latter.

All these values except SDRFC which seemed extra-baffling, and I don't think is the problem are from my reading of the Micron datasheet.

SDCFG: 0x08738A32 (note: it won't read back like this, because for some reason bit 27 for termination won't stay on. An older chip?

SDTIM1: 0x66DB5B49

SDTIM2: 0x017FC725

SDRFC: 0x0000073B (I just left this value the way it was)

The behavior is quite odd. I write to one location, my data shows up 2 words higher in memory. Most of it, anyway. Lower 16-bits seems favored over upper 16-bits, which means one chip is happier than the other. The upper byte of the upper word seems especially unhappy.

Anybody got a working GEL file for this configuration?