Other Parts Discussed in Thread: OMAPL138
HI,
I am using OmapL138 EVM Zoom Board. When i am connect to PC using XDS100v1(on board), I am getting this error
"Error connecting to the target
Error 0x80000224/-2131 Fatal Error during: Initialization, OCS, Control
Cannot able to access register at 0x00000000 "
When I am using external xds100v2 emulator I am getting error as
"Error connecting to the target
Error 0x80000224/-180 Fatal Error during: Initialization, OCS, Control
Cannot able to access register at 0x00000000"
Board is power up properly, S7 switch is set up in emu mode.
Thanks & regards,
Kalaiyarasan s