Other Parts Discussed in Thread: SK-AM64B
Hi,
I have observed the following issue with Ethernet on AM6442 when running TI kernel 6.1.46-rt13 (09.01.00.002-rt).
After this happens Ethernet communications are dead and require a reboot to function again.
[ 2826.211565] ------------[ cut here ]------------
[ 2826.211581] NETDEV WATCHDOG: eth0 (am65-cpsw-nuss): transmit queue 0 timed out
[ 2826.211650] WARNING: CPU: 0 PID: 11 at net/sched/sch_generic.c:525 dev_watchdog+0x254/0x260
[ 2826.211688] CPU: 0 PID: 11 Comm: ktimers/0 Not tainted 6.1.46-rt13 #1
[ 2826.211698] Hardware name:
[ 2826.211704] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 2826.211714] pc : dev_watchdog+0x254/0x260
[ 2826.211725] lr : dev_watchdog+0x254/0x260
[ 2826.211736] sp : ffff800008bb3c20
[ 2826.211739] x29: ffff800008bb3c20 x28: ffff8000085d2430 x27: ffff800008bb3d30
[ 2826.211755] x26: ffff00006fc23d50 x25: 0000000000000000 x24: 0000000000000000
[ 2826.211766] x23: ffff8000089b8000 x22: 0000000000000000 x21: ffff000001c683a0
[ 2826.211778] x20: ffff000001c68000 x19: ffff000001c68468 x18: ffffffffffffffff
[ 2826.211789] x17: 6f2064656d697420 x16: 3020657565757120 x15: 74696d736e617274
[ 2826.211801] x14: 203a297373756e2d x13: 74756f2064656d69 x12: 7420302065756575
[ 2826.211812] x11: 712074696d736e61 x10: 7274203a29737375 x9 : 777370632d35366d
[ 2826.211824] x8 : ffff8000089cb1f0 x7 : ffff800008bb3a30 x6 : 000000000000000c
[ 2826.211836] x5 : ffff00006fc23b40 x4 : 0000000000000000 x3 : 0000000000000027
[ 2826.211846] x2 : 0000000000000000 x1 : 0000000000000000 x0 : ffff000000cd8d80
[ 2826.211858] Call trace:
[ 2826.211862] dev_watchdog+0x254/0x260
[ 2826.211874] call_timer_fn.constprop.0+0x20/0x80
[ 2826.211891] __run_timers+0x270/0x2f0
[ 2826.211902] run_timer_softirq+0x1c/0x40
[ 2826.211913] _stext+0xf4/0x228
[ 2826.211922] run_timersd+0x60/0xc0
[ 2826.211935] smpboot_thread_fn+0x278/0x2e0
[ 2826.211945] kthread+0x110/0x120
[ 2826.211953] ret_from_fork+0x10/0x20
[ 2826.211963] ---[ end trace 0000000000000000 ]---
[ 2826.211983] am65-cpsw-nuss 8000000.ethernet eth0: txq:0 DRV_XOFF:0 tmo:5660 dql_avail:-2 free_desc:509
[ 2831.331490] am65-cpsw-nuss 8000000.ethernet eth0: txq:0 DRV_XOFF:0 tmo:10780 dql_avail:-2 free_desc:509
[ 2837.219386] am65-cpsw-nuss 8000000.ethernet eth0: txq:0 DRV_XOFF:0 tmo:16668 dql_avail:-2 free_desc:509
[ 2842.083298] am65-cpsw-nuss 8000000.ethernet eth0: txq:0 DRV_XOFF:0 tmo:21532 dql_avail:-2 free_desc:509
[ 2847.203202] am65-cpsw-nuss 8000000.ethernet eth0: txq:0 DRV_XOFF:0 tmo:26652 dql_avail:-2 free_desc:509
[ 2852.323117] am65-cpsw-nuss 8000000.ethernet eth0: txq:0 DRV_XOFF:0 tmo:31772 dql_avail:-2 free_desc:509
[ 2858.211011] am65-cpsw-nuss 8000000.ethernet eth0: txq:0 DRV_XOFF:0 tmo:37660 dql_avail:-2 free_desc:509
[ 2863.330918] am65-cpsw-nuss 8000000.ethernet eth0: txq:0 DRV_XOFF:0 tmo:42780 dql_avail:-2 free_desc:509
[ 2869.218815] am65-cpsw-nuss 8000000.ethernet eth0: txq:0 DRV_XOFF:0 tmo:48668 dql_avail:-2 free_desc:509