Part Number: PROCESSOR-SDK-AM62X
Hi ,
trying to load the images (tiboot3.bin/ tispl.bin/ uboot.img) through uart . After u-boot.img loaded getting below errors .
SDK : 09.00.00.03
please find attached logs
please help me on this .
CC
U-Boot SPL 2023.04-00001-gf5b119738d (Oct 17 2023 - 16:58:21 +0530)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 13400 bytes
Trying to boot from UART
CCWarning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Loaded 1138859 bytes
Loading Environment from nowhere... OK
init_env from device 7 not supported!
Starting ATF on ARM64 core...
NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 00:42:57, Jan 13 2023
U-Boot SPL 2023.04-00001-gf5b119738d (Oct 17 2023 - 16:58:31 +0530)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 1904 bytes
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:1
Error: could not access storage.
Trying to boot from UART
CCWarning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Loaded 948899 bytes
U-Boot 2023.04-00001-gf5b119738d (Oct 17 2023 - 16:58:31 +0530)
SoC: AM62X SR1.0 GP
Model: Texas Instruments AM625 SK
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -121
DRAM: 2 GiB
Core: 71 devices, 31 uclasses, devicetree: separate
MMC: mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In: serial
Out: serial
Err: serial
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -121
Net: eth0: ethernet@8000000port@1
Hit any key to stop autoboot: 0
MMC: no card present
SD/MMC found on device 1
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1
Can't set block device
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1
Can't set block device
MMC: no card present
** Bad device specification mmc 1 **
## Error: "main_cpsw0_qsgmii_phyinit" not defined
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
Bad Linux ARM64 Image magic!
switch to partitions #0, OK
mmc0(part 0) is current device
Scanning mmc 0:1...
MMC: no card present
No EFI system partition
No EFI system partition
Failed to persist EFI variables
BootOrder not defined
EFI boot manager: Cannot load any image
Found EFI removable media binary efi/boot/bootaa64.efi
733184 bytes read in 25 ms (28 MiB/s)
Booting /efi\boot\bootaa64.efi
Welcome to GRUB!
error: no such device: ((hd0,msdos1)/efi/boot)/EFI/BOOT/grub.cfg.
error: serial port `com0' isn't found.
GNU GRUB version 2.06
lqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqk
x*boot x
x x
x x
x x
x x
x x
x x
x x
x x
x x
x x
x x
mqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqj
Use the ? and ? keys to select which entry is highlighted.
Press enter to boot the selected OS, `e' to edit the commands
before booting or `c' for a command-line.
The highlighted entry will be executed automatically in 0s.
Booting `boot'
EFI stub: Booting Linux Kernel...
EFI stub: EFI_RNG_PROTOCOL unavailable
EFI stub: Using DTB from configuration table
EFI stub: Exiting boot services...
ti_sci system-controller@44043000: ti_sci_get_response: Message receive failed. ret = -110
ti-sci-pm-domains power-controller: ti_sci_power_domain_off: put_device(186) failed (-110)
ERROR: Timeout waiting for thread SP_RESPONSE to fill
ERROR: Thread SP_RESPONSE verification failed (-60)
ERROR: Message receive failed (-60)
ERROR: Failed to get response (-60)
ERROR: Transfer send failed (-60)
ERROR: Request to start core failed: -60
ERROR: Timeout waiting for thread SP_RESPONSE to fill
ERROR: Thread SP_RESPONSE verification failed (-60)
ERROR: Message receive failed (-60)
ERROR: Failed to get response (-60)
ERROR: Transfer send failed (-60)
ERROR: Request for processor failed: -60
ERROR: Timeout waiting for thread SP_RESPONSE to fill
ERROR: Thread SP_RESPONSE verification failed (-60)
ERROR: Message receive failed (-60)
ERROR: Failed to get response (-60)
ERROR: Transfer send failed (-60)
ERROR: Request for processor failed: -60