This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 USB



hii,

I am trying to do CSL_USB_PollExample on EZDSP board  using with USB host tool. i installed USB host tool like:

1.0. open a DOS command window and type in the following commands

1.1. wdreg -inf C5505USB_EP_driver.inf install

1.2. wdreg -inf C5505USB_EP_device.inf preinstall

1.3. copy "wdapi1010.dll" to %windir%\system32 (C:\Windows\SysWoW64  for 64 bit machine)

I am facing some problems:

 Problem1:I tried on 64 bit machine(64bit OS windows 7) when double clicked on c5505usb_ep_diag.exe file i am not getting popup.

 Problem2:I tried on 64 bit machine(32 bit OS windows 7) i am getting popup but its giving on dos prompt: Please make sure that the device is connected

what might be the problem?

Is problem with 64-bit machine or 64-bit os?

thanks &regards

Ramanjulu