Other Parts Discussed in Thread: SYSBIOS
I am developing code for C6678 involving multicore communications/synchronization. Now I encoutered a problem, i.e., using GateMP will fail if Intc is intialized. The tool chain I am using is listed below:
MCSDK: 2.0.1.12
C6678 PDK: 1.0.0.12
IPC: 1.23.0.26
Sys/BIOS: 6.32.01.38
XDC: 3.22.01.21
TI Compiler: 7.3.0
CCS: 5.0.3.00028
The two files at the end of this posting should reproduce the problem. The problem is that calling CSL_intcInit before calling GateMP_open() by cores 1 to 7 will cause failure in finding the named GateMP created by core 0. If I comment out the line calling InitIntc() in tsk0_func, calling GateMP_open(0 will succeed after a few loop iterations. Another (related) problem is if I do Intc initialzation after all cores have the GateMP opened, then using the GateMP will causes an assertion failure for cores 1 to 7 with the error message:
ti.sdo.ipc.GateMP: line 208: assertion failure: A_nullArgument: Required argument is null I would be very grateful for reasons of and solutions to the problem. Dongning
--------------------------------- main.cpp -------------------------------
#include <xdc/std.h>
#include <string.h>
#include <xdc/runtime/System.h>
#include <ti/ipc/Ipc.h>
#include <ti/ipc/MultiProc.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <xdc/cfg/global.h>
#include <ti/ipc/GateMP.h>
#include <ti/csl/src/intc/csl_intc.h>
static Char gateMpName[] = "myGateMpName";
static int regionId = 0;
CSL_IntcContext intcContext;
enum{
NUM_INTCS = 2, // Only INTC0 and INTC1 can generate interrupt to core
NUM_HANDLERS = 10
};
CSL_IntcEventHandlerRecord EventHandler[NUM_HANDLERS];
void InitIntc(Int32 intcNum)
{
if(intcNum < 0 || intcNum >= NUM_INTCS)
{
System_printf("There are only 4 INTCs!");
return;
}
intcContext.eventhandlerRecord = EventHandler;
intcContext.numEvtEntries = NUM_HANDLERS;
if (CSL_intcInit(&intcContext) != CSL_SOK)
{
System_printf("Error: GEM-INTC initialization failed\n");
return;
}
}
extern "C" Void tsk0_func(UArg arg0, UArg arg1)
{
int coreId = MultiProc_self();
System_printf("tsk0_func%d\n", coreId);
InitIntc(coreId >> 2);
Int status;
GateMP_Handle m_handle = NULL;
if (MultiProc_self() == 0) {
GateMP_Params params;
GateMP_Params_init(¶ms);
params.localProtect = GateMP_LocalProtect_THREAD;
params.remoteProtect = GateMP_RemoteProtect_SYSTEM;
params.name = gateMpName;
params.regionId = regionId;
m_handle = GateMP_create(¶ms);
System_printf("GateMP_create(%08x)\n", m_handle);
}
else {
do {
status = GateMP_open(gateMpName, &m_handle);
if (status < 0) {
Task_sleep(1);
}
} while (status < 0);
System_printf("GateMP_open(%08x)\n", m_handle);
}
System_printf("The test is complete\n");
}
Int main(Int argc, Char* argv[])
{
Int status = Ipc_start();
if (status < 0) {
System_abort("Ipc_start failed\n");
}
BIOS_start();
return (0);
}
------------------------ cfg file ----------------------------------
switch (Program.platformName) {
case "ti.sdo.ipc.examples.platforms.evm6670.core0":
var nameList = ["CORE0", "CORE1", "CORE2", "CORE3"];
break;
case "ti.sdo.ipc.examples.platforms.evm6678.core0":
var nameList = ["CORE0", "CORE1", "CORE2", "CORE3",
"CORE4", "CORE5", "CORE6", "CORE7"];
break;
case "ti.platforms.evm6678":
var nameList = ["CORE0", "CORE1", "CORE2", "CORE3",
"CORE4", "CORE5", "CORE6", "CORE7"];
break;
default:
throw("Platform " + Program.platformName + " not supported by this example");
break;
}
var Timestamp = xdc.useModule('xdc.runtime.Timestamp');
var GateMP = xdc.useModule('ti.sdo.ipc.GateMP');
var Settings = xdc.useModule('ti.csl.Settings');
Settings.useCSLIntcLib = true;
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
MultiProc.setConfig(null, nameList);
/*
* The SysStd System provider is a good one to use for debugging
* but does not have the best performance. Use xdc.runtime.SysMin
* for better performance.
*/
var System = xdc.useModule('xdc.runtime.System');
var SysStd = xdc.useModule('xdc.runtime.SysStd');
System.SupportProxy = SysStd;
var Ipc = xdc.useModule('ti.sdo.ipc.Ipc');
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
/* BIOS/XDC modules */
var BIOS = xdc.useModule('ti.sysbios.BIOS');
BIOS.heapSize = 0x8000;
var Task = xdc.useModule('ti.sysbios.knl.Task');
var tsk0 = Task.create('&tsk0_func');
tsk0.instance.name = "tsk0";
/* Synchronize all processors (this will be done in Ipc_start) */
Ipc.procSync = Ipc.ProcSync_ALL;
/* Shared Memory base address and length */
var SHAREDMEM = 0x0C000000;
var SHAREDMEMSIZE = 0x00200000;
/*
* Need to define the shared region. The IPC modules use this
* to make portable pointers. All processors need to add this
* call with their base address of the shared memory region.
* If the processor cannot access the memory, do not add it.
*/
var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
SharedRegion.setEntryMeta(0,
{ base: SHAREDMEM,
len: SHAREDMEMSIZE,
ownerProcId: 0,
isValid: true,
name: "DDR2 RAM",
});
/*
* @(#) ti.sdo.ipc.examples.multicore.evm667x; 1, 0, 0, 0,86; 6-18-2011 17:34:50; /db/vtree/library/trees/ipc/ipc.git/src/ ipc-g26
*/