Other Parts Discussed in Thread: AM1808, OMAP-L138, CCSTUDIO
Datasheet for AM1808 (SPRS653B) does not list SD Card as a possible
boot
option.
It says to look at (SPRAB41) for more info. SPRAB41D it
titled "Using
the OMAP-L138 Bootloader. This document
Boot Mode Selection
Table lists MMC/SD0 as a possible option with
footnote "MMC/SD boot mode is
only supported by ROM revision d800k008.
To check your ROM revision, follow
the instructions in Section 1."
Also in the SPRABA5B "Using the AM18xx
Bootloader" it says the same
thing about MMC/SD0.
It looks to me that it may have been a late
addition to the boot ROM in the AM1808. I would like
to know when this
change was made and if it is something that will be
kept in any future
versions of the ROM.
Can we safely design using
the MMC/SD0 as a boot option today or would
we have to worry that the parts
we buy might have an incompatible
version of ROM.
If yes, is there a date code on the part that we make sure it is compatible part ???