Part Number: SK-AM62B
Environment:
1)SK-AM62B
2)SDK ti-processor-sdk-linux-rt-am62xx-evm-08.06.00.42
Test:
first,i connect the sk-am62b by using the usb cable on the type-C(J13)
then i run the as the following command under the uboot,
=> fastboot 0
and i run the command under the window,but there is no any responding (however i run the fastboot 0 repeatly)
D:\Program Files (x86)\Fastboot-tools>fastboot.exe device < waiting for any device >
i check the Window DeviceManager,it found that as the following prompt

Issue:
1 can you provide the <USB download gadget> driver ?
2 or can you tell me that how to use the fastboot to connect the am62(in the uboot) and PC?