This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Device memory bus has an error and may be hung...



Hi all,

- I get the following error when debugging my c5505 board. I've lowered TCLK(up to 10khz) as it requests but it didn't work

C55xx: Can't Single Step Target Program: (Error -2130 @ 0x400) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Release 5.0.333.0) 

C55xx: Trouble Reading PC Register: (Error -1143 @ 0x0) Device memory bus has an error and may be hung. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Release 5.0.333.0)

 

- I get these errors when I step over  the instruction below 

SPI_SPICCR = 0x0000; // SPI clock disabled              ( SPI_SPICCR   has address of 0x3001)

- Same error exists for other spi registers when I step them over. Also when I view the memory, I see BAD mark beginning  from 0x3000's.

- There is no problem when I debug demo boards on which they have VC5505, but problem arises on my C5505 board.

- I know they have the same register address

- What could be the reason?

Thanks...