This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: Is there an accumulated max number of tensors?

Part Number: TDA4VH-Q1

Hello,

I have multiple models and the accumulated number of tensors is 128.

And I got an error "May need to increase the value of TIVX_TENSOR_MAX_OBJECTS in tiovx/include/TI/tivx_config.h"

I am not sure it is about max number of each model file or the accumulated number.

Secondly, the TIVX_TENSOR_MAX_OBJECTS is 256, so it is less than 128.

Could you advise me?

Best regards,