This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AL-Q1: unable to select a mode : -5 /spl: mmc init failed with error: -524 / SPL: failed to boot from all boot devices

Part Number: TDA4AL-Q1
Other Parts Discussed in Thread: CSD

Dear Sir,

      My Board print following error log and can not run when we are doing Temperature Experiment on -10℃. What's the reason for the error log: unable to select a mode : -5 /spl: mmc init failed with error: -524 / SPL: failed to boot from all boot devices

U-Boot SPL 2021.01(Nov 08 2023 - 19:25:27 +0800)
i sci system-controller@44083000: Message not acknowledgedSYSFW ABl: 3.1 (firmware rev 0x0008 8.6.3--08.06.03 (Chil Capybar"
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -19
SPL initial stack usage: 13472 bytes
Irying to boot from MMC1
unable to select a mode : -5
spl: mmc init failed with error: -524
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###