Hi I'm using Raw 12bit monochrome IR sensor.
I would like to use NSF3V, GLBCE, and 2D-Edge Enhancer. So I set the ipipe path to "raw to yuv422". However, when I input 0xFFF data, the image output seems to be cut off. The output is very low data (0x46).
My guess is that the CFA module is causing this problem. I understand how RGB2RGB1, gamma, RGB2RGB2, and RGB2YUV modules work. But I don't know how the CFA module works.
In summary, I am wondering if it is possible to use the route of using CFA when using Raw 12bit monochrome format. If possible, I would like to know if there is a manual or explanatory material for the CFA module.
Best regards