Part Number: AM625
Other Parts Discussed in Thread: AB15, TEST2
Hi,
Please refer to below that we use the AM6254, and please advise why this core kernel crash, thanks.

The below is the print imformation:
root@am62xx-evm:~#
root@am62xx-evm:~# [ 2833.974238] usb 1-1.3: USB disconnect, device number 3
[ 2834.149302] FAT-fs (sda1): unable to read boot sector to mark fs as dirty
[21251.654469] ------------[ cut here ]------------
[21251.659111] kernel BUG at arch/arm64/kernel/traps.c:407!
[21251.664416] Internal error: Oops - BUG: 0 [#1] PREEMPT SMP
[21251.669895] Modules linked in: xt_conntrack xt_MASQUERADE xt_addrtype iptable_filter iptable_nat nf_nat nf_conntrack nf_defrag_ipv6 nf_defrag_ipv4 libcrc32c ip_tables x_tables br_netfilter bridge stp
llc overlay xfrm_user xfrm_algo md5 des_generic libdes cbc wlcore_sdio wl18xx wlcore mac80211 cfg80211 rfkill libarc4 usbhid usb_storage xhci_plat_hcd xhci_hcd usbcore dwc3 udc_core rpmsg_char
roles usb_common cdns_csi2rx v4l2_fwnode pru_rproc irq_pruss_intc pvrsrvkm(O) crct10dif_ce ti_k3_r5_remoteproc virtio_rpmsg_bus dwc3_am62 rti_wdt j721e_csi2rx videobuf2_dma_contig videobuf2_memops
videobuf2_v4l2 videobuf2_common sa2ul pruss sha512_generic authenc cdns_dphy mcrc rtc_ds1307 sch_fq_codel cryptodev(O) ipv6
[21251.732352] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G O 5.10.168-g2c23e6c538 #1
[21251.740861] Hardware name: LICHAN Texas Instruments AM625 SK (DT)
[21251.746942] pstate: 00000085 (nzcv daIf -PAN -UAO -TCO BTYPE=--)
[21251.752948] pc : do_undefinstr+0x2f4/0x318
[21251.757036] lr : do_undefinstr+0x1e8/0x318
[21251.761119] sp : ffff80001132be00
[21251.764421] x29: ffff80001132be00 x28: ffff8000111919c0
[21251.769723] x27: ffff8000111919c0 x26: ffff80001132c000
[21251.775025] x25: ffff800011328000 x24: ffff800011189a54
[21251.780326] x23: 0000000040000085 x22: ffff80001052b940
[21251.785626] x21: ffff80001132bfe0 x20: ffff8000111919c0
[21251.790926] x19: ffff80001132be90 x18: 0000000000000000
[21251.796226] x17: 0000000000000000 x16: 0000000000000000
[21251.801527] x15: ffff80001052b940 x14: 0000000000000099
[21251.806827] x13: 0000000000000000 x12: 0000000000000001
[21251.812127] x11: 0000000000000000 x10: 0000000000