AM5728: AM5728 QSPI data transmission is not continuous.

Part Number: AM5728

I have observed that the process of downloading files in the configured environment, which involves AM5728 and a flash memory (S25FL256S), is much slower than the configured speed. When measured with a scope, I have confirmed the presence of continuous blank periods during data transmission.

It seems that there are limitations to improving the speed by modifying only the SPI_defaultParams provided in the PDK code for the S25FL. If there are additional options or settings that need to be configured, I would appreciate it if you could provide that information.