This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: PHY driver issue

Part Number: TDA4VH-Q1


Hi Team,

1) PHY chip boot status issue. Will the DP83TG720S and DP83TC812S enter normal state after the original power-on reset and hardware reset of the DP83867? Does the code need to be adjusted?

2) Configuration issues with PHY chip special registers. DP83TG720S and DP83TC812S have extended registers that are quite different from DP83867, the customer would like to know which registers need to be configured? In addition to initializing the Dp83867_config() function, which functions need to adjust the register configuration?

3) Is there any related examples available for reference?  Since only the driver examples under DP83TG720S and DP83TC812S Linux can be found.

Could you help look into these 3 issues? Thanks.

Best Regards,

Cherry