Part Number: TDA4VM
Hi TI Experts,
Customer is working on TDA4VM SDK8.6.
As we see from the below picture of DMPAC Data Flow with FOCO, the FOCO can convert the input data to 12-bit and written back into SL2 to be consumed by the SDE and DOF engines.

So it means that the output data format of DMPAC output is different from the input data if the input data is not 12-bit. If we want to convert the the DMPAC output data format back to be consistent with the input data format (not equal to 12 bit), how could we make it?
Seeing from the above picture, the FOCO seems can only do the one-way format conversion, so I assume it could not be used to convert the DMPAC output data back to the input format.
May I know if the FOCO technique is based on the purely hardware or there is software involved? If it is software involved, the 12-bit is just 2 bytes, can customers extract the 12-bit DMPAC output according to the address from high to low or from low to high? If not, any suggestions would be appreciated!
Kind Regards,
Kevin