Hello colleagues,
Is the video encoding engine of the AM68A are suitable to encode 8 CVBS (PAL (625i50) or NTSC (525i60)) to store data via USB Interface to a
SATA drive? The input of the CVBS would be via 2x CSI In with 4 lanes each.
Is the video decoding engine of the AM68A are suitable to decode up to 4 IP camera streams to display a quad screen (DSI)? Both RGMII interfaces will be used to get the IP streams.
In the datasheet it is mentioned that both engines are capable to process up to 4k60 with 480MP/s. But do they support multiple different video streams up to 480 MP/s in total?
Thank you,
Daria