Any recommendations on a driver for the CLK input on an OMAPL138, OSCIN pin.
As I understand it, OSCIN is a 1.2V level input, Vih = 0.96V, Vil = 0.24 and I am searching for a buffer to drive this input.
thanks
Paul
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Any recommendations on a driver for the CLK input on an OMAPL138, OSCIN pin.
As I understand it, OSCIN is a 1.2V level input, Vih = 0.96V, Vil = 0.24 and I am searching for a buffer to drive this input.
thanks
Paul
You may need to ask in the clock forum. What about using a crystal?
I took a quick look at our OMAPL138 Low Cost Development Kit (LCDK) schematics:
http://processors.wiki.ti.com/index.php/LCDK_User_Guide#Schematics
I also had a quick look at the companion guide:
http://processors.wiki.ti.com/index.php/OMAP-L138_LCDK_Schematic_Companion
It makes the following comment with regard to that clock (Y3):
So one option might be to simply do as they have done and use a voltage divider.
Brad,
I do not think it is advisable to drive a system clock by means of a resistor divider due to SI and EMI concerns.
I would like to meet the TI spec with a TI push-pull logic.
Thanks,
Milan