Other Parts Discussed in Thread: SEGGER, AM3359
Hi,
I want to use the ROV to debug my device. After connecting to the target and loading the application (debbuger has stopped at "main()"), I want to start up the ROV by pressing "Connect" (Executable path: "<Use the program currently being debugged>", Target communication link: "Debugger"). I then get following error:
Error: Failed to start ROV using 'comm=DSLite:1,wsPort=63714':: Can't extract RTSC configuration package path from 'path/to/application.out'.
I use following setup / toolchain:
- Code Composer Studio: v8.2.0.00007
- OS: TI-RTOS
- TI-BIOS v6.73.00.12
- Compiler: GNU v6.3.1 (Linaro)
- Output type: RTSC Application (Executable)
- Output format: eabi (ELF)
- XDCtools: 3.50.08.24
- Debugger: SEGGER J-Link
- Target Configuration
- Board or Device: ICE_AM3359
- Initialization script: emulation\board\ice_am3359\gel\TMDXICE3359.gel
Does anyone have an idea how I can solve that error message?