Part Number: TDA4VM
Dear TI experts,
I'm now creating a demonstration that using DSI on Linux to display some image/video (I'm not using the DSI in vision_apps demo with cameras).
Further, I also want to use DRM/Wayland/Weston with Qt also, but this is in next step.
The system can be show as below:

So firstly, I'd like to ask that is it possible to perform this implement with current support of TDA4VM SoC? I currently use the SDK 8.5.
If it possible, could you guide me some clues where I can begin?
I've read and tried with following ticket:
I understand that above ticket will disable the DSS on vision_apps and enable this on Linux.
I've this this one, but after that, I see that there are no DSI clock or data signal at all.
And with 3 tickets here:
I understand that this is the next step after I perform enable DSS on Linux. I need to
1 - Add display timing setting in 'drivers/gpu/drm/panel/panel-simple.c'
2 - Add device tree overlay to enable panel
But because this is first time I work with display on Linux so I still not really understand how to do that .
So could you please help correct my understand and clarify those steps above? E.g: How to create display timing? How to enable panel in device tree? (Most of the example and refs link in the ticket seems expires and I cannot access so not sure how to check the modification sources)
Thank you for your support.
Best regards,
Dinh.