Part Number: TMS320C6655
Other Parts Discussed in Thread: TMS320C6678
Hi,
We are using TM320C6655 DSP PROCESSOR and using gpio pins14 and 15 as an interrupt which corresponds to no 88 and 89 in primary interrupt event .In our application fpga triggers the interrupt in dsp .
For some time it is working fine. After certain triggers ,when fpga tries to give trigger signal , the dsp goes into nmi mode. If we have debug the same logic, every time it is in same state. Approximately in one board it is 42, time43rd time we are getting this error.
Whereas in another two boards with same configuration ,this issue is happening in 98th trigger and on 112th time and these happen constantly every time I reset the board and check .
Please check the issue and revert back for this query.


Regards,
Thilak