Part Number: SK-AM64
Hi
We want to use the following EVM;
https://www.ti.com/tool/SK-AM64#included
to evaluate the following application:
- To simultaneously acquire data from two SPI ports; a transaction each 0.2msec, 150 bytes each transaction from each port, clock speed of 8Mbits/sec
- This data is gathered in the Linux core and continuously sent in larger packets through wi-fi to a smart phone. Expecting a transfer rate of ~1.5Mbytes/sec.
Questions:
- Is the SK-AM64 good for this?
- Is the out of the box Wi-Fi board option is our starting point? Do you have libraries for WIFI on this SK-AM64?, Do we only need to do is program the SPI transactions and create the Wi-Fi blocks, and send through the wi-fi libraries of the SK-AM64?
- planning future to use the onboard USB to connect to host and stream the data, is that possible? and how complicated should we expect it to be to get it working ?
Best Regards,
Jameel