Part Number: SK-AM69
Unfortunately, both of the following SDKs (regular WIC images flashed to SD cards) fail on both our E3 SK-AM69 boards (regular HS-FS ones) while the previous version 08.06.01.03 (31 May 2023) still works fine:
PROCESSOR-SDK-LINUX-AM69
09.00.00.06 (29 Jul 2023)
and
PROCESSOR-SDK-LINUX-AM69A
09.00.01.03 (12 Oct 2023)
And this is the exact error one gets upon boot:
U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) EEPROM not available at 0x50, trying to read at 0x51 SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') SPL initial stack usage: 13424 bytes Trying to boot from MMC2 Authentication passed Authentication passed Authentication passed Authentication passed Authentication passed Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.9(release):v2.9.0-dirty NOTICE: BL31: Built : 14:12:59, May 22 2023 I/TC: I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Authentication passed ti_sci system-controller@44083000: Message not acknowledgedAuthentication failed! ### ERROR ### Please RESET the board ###
Please advice, thanks!