Hi,
We are using the DM6467 DSP for developing our set top box system.
The DSP bios version is 5.41
The ARM clock is set to 495Mhz whereas the DSP being twice the clock rate for ARM is set to approx 1GHz.
This basically leads to very high power consumption and additionally heats up the device in long run.
Additionally the DSP is used only for decoding digital streams hence it may not be necessary to clock the DSP at such a high rate
Hence my query is
1) Is is possible to change the DSP clock rate with out effecting the ARM clock since we do need the ARM clock to run at the at the same rate as mentioned above ie ca we change the clock ratio between ARM and DSP?
2) Additionally can we also the turn off the DSP clocks when we dont need them. (This has been asked already in a separate query on e2e for which the reply is still pending)
3) Does the DSP BIOS have an idle mode implementation whereby it can go to low power mode when not in use
Thanks and Regards
Mohammed Anwar