Part Number: CCSTUDIO
Hi CCS Experts,
We have found that there are 2 ways below in CCS to do system reset and clear the memory.
1: Click the System Reset Button

2: Reset the target on a connect

As customer is implementing a complete script to periodically run their application, for each time a system reset is needed. For the above two methods, they could both work to achieve this goal. However, they could not be merged to customer's script to automatically do system reset.
Hence, may I know if there is a CCS script available for any of the above two methods please?
Note this thread is only for system reset, not CPU reset.
Thanks a lot!
Kevin