Hi,
I have a quesion regarding SRAM connection using GPMC of AM3505.
According to the AM35x Technical Reference manual, the external memory interfaces support only limited address(2Kbytes) with no-mux mode.
If user would like to use a larger size SRAM, user can use an external latch to get the address un-muxed from the GPMC same as non-mux NOR flash, doesn't it?