This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-LCD1: SK-LCD1 Timing diagram

Part Number: SK-LCD1
Other Parts Discussed in Thread: SK-AM62B, SK-AM62-LP, SK-AM62, AM625

Hi

Regarding SK-LCD1,

I have searched the internet for information, but I did not find a Timing diagram similar to SK-LCD1.

Is there any other relevant information available?

13-101HIEB0HF0-S V1.0 20200507.doc (mouser.com)

  • Hello Vic Chang,

    The SK-LCD1 is a  10.1 inch OLDI LCD.

    https://www.ti.com/tool/SK-LCD1

    The 1920x1200 OLDI/LVDS LCD display accessory kit is an add-on accessory for the starter kit EVMs of AM62x processors (SK-AM62, SK-AM62B, SK-AM62-LP, etc), to add touch and display functions for the evaluation of HMI, industrial PC and other use cases requiring display. The TFT LCD screen is a 10.1" display with WUXGA resolution (1920x1200) and supports 10 point capacitive touch.

    Please refer to the AM625 data sheet for the available timing information.

    Regards,

    Sreenivasa