Hello,
with the eZDSP C5505 I`m clear, flashing works with "programmer_USBKey.out" and my generated *.bin file from the first "getting started" example from the CD: "TMS320C5505 USB Stick Teaching Materials".
The same example run on the eZDSP C5515 too (with some changes, for
example: --silicon_version,-v: cpu:3.3; and: Generic C55xxDevice), but
flashing that *.bin file with
"4011.programmer.out" doesn`t work, the eZDSP C5515 do nothing after it is reconnect.
With the "4011.programmer.out" I can run the "cleaner.bin" and the "EZDSP_Sample.bin" succesfully on eZDSP C5515.
What is wrong with my generated *.bin file from the "Getting Started-CD", the *.bin file is 24 KB ?
Thanks very much, I much appreciate your help,
cheers