Hi
I am using TMS320C6674 and have a question.
I am booting the DSP using EMIF Boot mode. There are no issues with the operation, but even when I change the Bootmode[12:10] PLL boot config setting, it continues to work fine.
According to the information in the datasheet, I understood that the Boot PLL varies depending on Bootmode[12:10].
Is my understanding correct, or does EMIF not affect the Boot PLL?
-TMS320C6674 datasheet(Please refer to the PLL Boot Configuration Setting in section 2.5.4.)