Other Parts Discussed in Thread: CCSTUDIO
I am using code composer 3.1 and Spectrum Digital XDS510 USB pod to program flash memory connected to a C6713 processor . On 2 out of the 4 workstations (if the flash memory is blank) that i try to program the flash memory with on our custom board, i get the following error: Error connecting to the tartet: Error 0x80000200/-1060
If the flash memory has an existing program already in memory I have no troubles programing, erasing, or connecting to target. If I erase the memory and then reset the board the problem of not being able to connect to target comes back on 2 out of the 4 workstations. I have used the same pod on different workstations so I don't think the pod is the issue. I have used the same driver on all systems and have gone as far as to copy the entire code composer directory between working and non working system and still get the same behavior. Can any one help me out. I am using a variety of workstations and have not found anything conclusive on this funny behavior.
Has any one seen this type of behavior? any suggestions?