This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Target directory changes from PSP 4.00.00.10 to PSP 4.00.00.12?

I realize that I'm jumping the gun here, but as I'm having Syslink problems I have gone to the latest version, 2.00.02.80, and to use it with the latest PSP, 4.00.00.12, with the in-kernel notify, I see that there are a different number of modules and the kernel 2.6.37+ is referred to.  How has the target directory structure changed going from PSP 4.00.00.10 to 4.00.00.12?  I rebuilt syslink and the new uImage did not find it.  I started out with EZSDK 5.01.01.80.

Lee Holeva