Hi,
The NIMU ethernet driver provided in the PDK of C6670 is compiled with the following defines (defined in resource_mgr.h):
#define NIMU_NUM_TX_DESC 16u /**< Maximum number of TX descriptors used by NIMU */
#define NIMU_NUM_RX_DESC 18u /**< Maximum number of RX descriptors used by NIMU */
#define MAX_NUM_NIMU_DESC (NIMU_NUM_TX_DESC + NIMU_NUM_RX_DESC) /**< Maximum number of descriptors used bye NIMU */