This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A problem about using PCIe ×1 of C6670

    Hi all

    As we know, there is a PCIe ×2 interface in C6670. But as the user guide saying, "The PCIe subsystem has only one interface link and this link can be used in ×1 or ×2 lane arrangements connecting to only one device. In other words, there exists no support for connecting to two devices in an ×1 arrangement since it has the support of a single interface link. It also means that it can not be used as a switch." And here is the problem, if I just want to use the interface as a ×1 lane arrangement, can I choose which lane to use? That is, can I choose lane 0 or lane 1 as the ×1 arrangement lane? And how to make it done? Thx