Hi, i'm trying to boot the am64-sk using sd card with linux default image tisdk-default-image-am64xx-evm.wic.xz .
I have also changed boot partition as mentioned here (On AM64x devices, the bootable SD card image may also have tiboot3-am64x-gp-evm.bin in the boot partition of the SD card image. Renaming tiboot3-am64x-gp-evm.bin to tiboot3.bin and removing/renaming the pre-existing tiboot3.bin of HS-FS type is the only change needed to run the HS-FS SDK on a GP board.)
but,im facing this issue please help me with this.
Type [C-a] [C-h] to see available commands
Terminal ready
�
U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
EEPROM not available at 0x50, trying to read at 0x51
Resetting on cold boot to workaround ErrataID:i2331
Please resend tiboot3.bin in case of UART/DFU boot
resetting ...
Thanks,
Prasanth.