This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: AM62A LP u-boot ethaddr value is different from the value written on the EVK circuit board.

Part Number: AM62A7


Hello, I am developing an AM62A SKEVM board.

I found something strange while working on it.

The MAC address written on the Ethernet connector and the ethaddr address shown in the U-BOOT are different.

Please help me.

  • Hi,

    Could you please share the two MAC addresses that you see? I don't have a board handy at the moment to reproduce the problem you see. Why I am asking is I am curious if both addresses were purchased by TI or if one is a random number.

    Other than the two addresses not matching what is the concern that you have? 

    Which TI SDK are you using and are you using the pre-built images from that SDK.

    Best Regards,

    Schuyler

  • Hi,

    The MAC address attached to the LAN connector on the motherboard is 70 FF 761F 1E 0C.

    However, the MAC address displayed through the U-BOOT is 1c:63:49:17:20:08.

    The firmware image is the prebuild image contained in the SDK.

    I read eeprom with the i2c command, but the MAC address was only 70 FF 761F 1E 0C written on the board.

    Thank you for your interest.

  • Hi,

    Thank you for posting the different MAC addresses.

    Both MAC addresses were purchased by TI. As you have noticed the EEPROM MAC address matches the label on the board. u-boot is using is the internal one that is programmed as the device is tested. 

    You can verify the 1c:63:49:17:20:08 MAC address is internal to the device by using the devmem2 command:

    devmem2 0x43000200 --- this is the least significant 4 bytes of the MAC address

    devmem2 0x43000204 --- this is the most significant 2 bytes of the MAC address

    The reason for the two addresses is that U-Boot as it boots reads the EEPROM MAC address it is passed to the kernel as a boot parameter. This serves as an example on how to read in a MAC addresses so when you design your board you do not have to use the MAC address in the device but rather one your company may purchase.

    Best Regards,

    Schuyler

  • Thank you. Thanks to you, my curiosity has been solved.

    An error occurs when trying to read the corresponding area with the "md" command of the U-BOOT, is it blocked by the security function?

    If it's a security function, is it ATF?

  • Hi, 

    Could you please post the console log showing this issue?

    Best Regards,

    Schuyler

  • I'm sorry.
    I think there was a mistake the other day.
    It works well now.
    Thank you.

    U-Boot SPL 2023.04-dirty (Dec 11 2023 - 08:55:53 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.5--v09.01.05 (Kool Koala)')
    am62a_init: board_init_f done
    SPL initial stack usage: 17032 bytes
    am62a_init: spl_boot_device: devstat = 0x24b bootmedia = 0x9 bootindex = 0
    Trying to boot from MMC1
    am62a_init: spl_boot_device: devstat = 0x24b bootmedia = 0x9 bootindex = 0
    Authentication passed
    am62a_init: spl_boot_device: devstat = 0x24b bootmedia = 0x9 bootindex = 0
    Authentication passed
    am62a_init: spl_boot_device: devstat = 0x24b bootmedia = 0x9 bootindex = 0
    Authentication passed
    am62a_init: spl_boot_device: devstat = 0x24b bootmedia = 0x9 bootindex = 0
    Authentication passed
    am62a_init: spl_boot_device: devstat = 0x24b bootmedia = 0x9 bootindex = 0
    Authentication passed
    Starting ATF on ARM64 core...

    NOTICE: BL31: v2.9.0 (release):v2.10-rc0-4-g5e52433dd
    NOTICE: BL31: Built : 09:10:56, Nov 14 2023
    ERROR: Failed to get response (-19)
    ERROR: Transfer send failed (-19)
    ERROR: Unable to query firmware capabilities (-19)
    I/TC:
    I/TC: OP-TEE version: 4.0.0-54-gb501c0084 (gcc version 11.3.1 20220712 (Arm GNU Toolchain 11.3.Rel1)) #1 Tue Nov 14 05:02:26 UTC 2023 aarch64
    I/TC: WARNING: This OP-TEE configuration might be insecure!
    I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
    I/TC: Primary CPU initializing
    I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.5--v09.01.05 (Kool Koala)')
    I/TC: HUK Initialized
    I/TC: Activated SA2UL device
    I/TC: Enabled firewalls for SA2UL TRNG device
    I/TC: SA2UL TRNG initialized
    I/TC: SA2UL Drivers initialized
    I/TC: Primary CPU switching to normal world boot

    U-Boot SPL 2023.04-dirty (Dec 11 2023 - 08:56:02 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.5--v09.01.05 (Kool Koala)')
    am62a_init: board_init_f done
    am62a_init: spl_boot_device: devstat = 0x24b bootmedia = 0x9 bootindex = 0
    Trying to boot from MMC1
    am62a_init: spl_boot_device: devstat = 0x24b bootmedia = 0x9 bootindex = 0
    Authentication passed
    am62a_init: spl_boot_device: devstat = 0x24b bootmedia = 0x9 bootindex = 0
    Authentication passed


    U-Boot 2023.04-dirty (Dec 11 2023 - 08:56:02 +0000)

    SoC: AM62AX SR1.0 HS-FS
    Model: Texas Instruments AM62A7 SK
    DRAM: 2 GiB (effective 4 GiB)
    Core: 58 devices, 28 uclasses, devicetree: separate
    MMC: mmc@fa10000: 0, mmc@fa00000: 1
    Loading Environment from nowhere... OK
    In: serial@2800000
    Out: serial@2800000
    Err: serial@2800000
    Net: eth0: ethernet@8000000port@1
    Hit any key to stop autoboot: 0
    =>
    =>
    =>
    => md 0x43000200 1
    43000200: 49172008 . .I
    => md 0x43000204 1
    43000204: 00001c63 c...
    =>