Other Parts Discussed in Thread: AM3505
Hi,
Our device has WAN module connected to SDIO interface on TI AM3505 with 2.6.32 kernel
The set up is as follows: PC is connected to our device via Ethernet or USB (Ethernet over USB) and a WAN module connected to SDIO interface
When running iPerf from the Ethernet interface to the WAN module we get 10% - 15% degradation in data transfer as compared to the USB to the WAN configuration.