I am using CCS 5.03 with a Blakhawk XDS560v2-USB Mezzanine emulator and an EVMc6678LE board. For some reason, when I opened up the project today, it showed an error on the ccxml file. It says there are no debuggable cpus.
I have tried to fix the ccxml, and then to generate a new one, but the C6678 is no longer in the list of devices. Previously, I had been abe to select the evm, but that dissapeared when I changed from runing on the XDS100 to the 560. I had been using the C6678 cpu from the list, but now that has gone too. I have a full licence, and CCS shows this if I look at licence status.
Any suggestions would be welcome.