Other Parts Discussed in Thread: ASH
In the serial I/O console for the EVM, the shell does not appear to have pathname expansion enabled. Is it possible to turn it on?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ASH
In the serial I/O console for the EVM, the shell does not appear to have pathname expansion enabled. Is it possible to turn it on?
It does not happen to me. I have my c6678 up using NAND boot. I got the following
/ #
/ # cd proc/fs
/proc/fs # cat /proc/cpuinfo
CPU: C66x
Core revision: 0x0
Core voltage: 1.2
Core id: 0
SoC cores: 8
MMU: none
FPU: yes
Silicon rev: unknown
Clocking: 1000MHz
BogoMips: 999.42
Calibration: 1998848 loops
/proc/fs #
I get the same results as you for the above commands, but I don't see what that has to do with how the shell is acting.
An example of what I am mentioning is:
/ # ls /bin/*
ls: /bin/*: No such file or directory
but ls works if I don't specify path expansion characters:
/ # ls -1 /bin
addgroup
...
Also I can't set the parameter to enable pathname expansion
/ # set +f
sh: set: +f: invalid option
And some builtins like getopts are not available
Is this a matter of how the shell is configured in busybox?
Hi,
I don't think "set" is an option can be enabled during the build, but getopt or getopts may be. The .config file in linux-c6x-project/busybox_config provides what can be built into busybox. I do see GETOPT and ASH_GETOPTS are options but currently disabled, but don't know if we really want to enable ASH_GETOPTS. I don't see anywhere to enable path expansion. All "ls" features are enabled. It could mean that path expansion is not supported unless I miss the config define in the .config file.
Rex