Hi, I'm hitting a problem where it appears that boot-time copy tables are not processed when the application boots through the QSPI SBL. If I load the application image through the JTAG debug port, then the copy tables are processed.
I have a minimal project that reproduces this issue that I can deliver as a .zip on request. I'm having difficulty sharing the entire example through the forum.
The example is based on the hello_world nortos example with two main changes.
First, I change hello_world.c to print a data string stored in a special program section allocated in RAM instead of a fixed string:
// Initialize some data in a special .data.test section
__attribute__((section(".data.test")))
static char data_section_string[] = "Hello World from .data.test!";
// ...
DebugP_log("[%s]\r\n", data_section_string);
Second I change linker.cmd to declare the .data.test section with a boot time copy table. I set up the load and run locations for this section to point to different addresses in OCRAM to keep the example simple.
SECTIONS
{
.binit > OCRAM
/* This is my special section that's initialized by a boot-time copy table */
GROUP: load = OCRAM1, run = OCRAM, table(BINIT) {
.data.test: {} palign(8)
}
...
}
Memory
{
...
OCRAM : ORIGIN = 0x70040000 , LENGTH = 0x40000
OCRAM1 : ORIGIN = 0x70140000 , LENGTH = 0x40000
}
I expect __TI_auto_init() to initialize the .data.test section on boot in any case, but when I load the application from the QSPI SBL packaged with MCU+SDK, I see the following output which shows that this data was not initialized.
Image loading done, switching to application ... []
I'm using LP-AM263 hardware, tiarmclang v3.2.0 and MCU+SDK 9.0.0.35
Thanks for taking a look