This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EZSDK pre-built image fail to run on DM8168-based DVR

I use pre-bilt image insdie ezsdk_05_01_01_80 and fail to boot up DM8168-based DVR.

it'll shutdown as booting kernel....

Any idea? Thanks

  • Hello,

    Can you please provide more details on what you see as it boots?

    Regards,
    Marc

  • See below for log:

     

    U-Boot 2010.06 (May 13 2011 - 01:05:43)

    TI8168-GP rev 1.1

    ARM clk: 987MHz
    DDR clk: 796MHz

    I2C:   ready
    DRAM:  2 GiB
    NAND:  256 MiB
    Net:   Ethernet PHY: GENERIC @ 0x01
    DaVinci EMAC
    Hit any key to stop autoboot:  0
    UBOOT # set nfsserver 192.168.2.173;set ipaddr 192.168.2.161;set gatewayip 192.168.107.254;set netmask 255.255.252.0;set serverip 19                         2.168.2.173;setenv bootargs 'console=ttyO2,115200n8 root=/dev/nfs nfsroot=192.168.2.173:/usr/local/ezsdk_05_01_01_80/filesystem/rfs,                          nolock rw mem=128M vram=20M earlyprintk ip=dhcp';tftp 81000000 uImage_EZSDK;bootm 81000000
    Connect speed 1G Full
    Using DaVinci EMAC device
    TFTP from server 192.168.2.173; our IP address is 192.168.2.161
    Filename 'uImage_EZSDK'.
    Load address: 0x81000000
    Loading: T #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #######
    done
    Bytes transferred = 2362144 (240b20 hex)
    ## Booting kernel from Legacy Image at 81000000 ...
       Image Name:   Arago/2.6.37-psp04.00.00.10/dm81
       Created:      2011-06-01   6:49:05 UTC
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2362080 Bytes = 2.3 MiB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.
    Linux version 2.6.37 (x0029463@swubn01) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Wed Jun 1 12:18:59 IST 2011
    CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
    CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
    Machine: ti8168evm
    vram size = 20971520 at 0
    bootconsole [earlycon0] enabled
    reserved size = 20971520 at 0
    FB: Reserving 20971520 bytes SDRAM for VRAM
    Memory policy: ECC disabled, Data cache writeback
    OMAP chip is TI8168 1.1
    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 27392
    Kernel command line: console=ttyO2,115200n8 root=/dev/nfs nfsroot=192.168.2.173:/usr/local/ezsdk_05_01_01_80/filesystem/rfs, nolock rw mem=128M vram=20M earlyprintk ip=dhcp
    PID hash table entries: 512 (order: -1, 2048 bytes)
    Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
    Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
    Memory: 108MB = 108MB total
    Memory: 104376k/104376k available, 26696k reserved, 0K highmem
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
        DMA     : 0xffc00000 - 0xffe00000   (   2 MB)
        vmalloc : 0xc8800000 - 0xf8000000   ( 760 MB)
        lowmem  : 0xc0000000 - 0xc8000000   ( 128 MB)
        modules : 0xbf000000 - 0xc0000000   (  16 MB)
          .init : 0xc0008000 - 0xc0035000   ( 180 kB)
          .text : 0xc0035000 - 0xc0478000   (4364 kB)
          .data : 0xc0478000 - 0xc04b91e0   ( 261 kB)
    SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    NR_IRQS:407
    IRQ: Found an INTC at 0x

    And then it shutdown automatically. Any idea?

  • hi friends,
        Any update?

     

  • Hi,

    What platform (i.e. boards and daughtercard combination) are you working with?

    Which version of the ezsdk are you using?

    Assuming it is DM816x Base EVM, can you successfully boot from the SD card using all pre-built images?

    Does this issue only occurs when booting over the network?

    Where is u-boot booting from and is it consistent with the kernel version you are using (i.e. from the same ezsdk/psp package)?

     

    Regards,

    Benoit

     

    P.S. If this response helps answer your question please mark this post as verified - Thanks