This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using SLAA210A to connect ths1206evm with a C6711

I want to communicate with a THS1206evm (slau042b.pdf) from a C6711 DSK , and have tried using the example in SLAA210A.

 

My question is: how do you determine the ADC Address which should be entered in the Data Converter Support (DCP) tool, which creates the files used in a program to call the functions such as dc_configure(), anddc_readblock()?

It seem like the DSp does not read anything.

 

I use this configuration:

Interface Settings                                         ADC Settings

 

ADC Address - 0xA0000000                      Channel Set:                   Autoscan 4 SE

Data Shift        - 0                                           Conversion Clock:         6000 kHz

DATA_AV Polarity - High                              Mode                                 Continuous Conversion

Data_AV Type       - Pulse                            Trigger Level                    4

Read/Write Type  - RD/WR                          Test Mode                        Normal Mode

Data Format         - Binary                                  Ref Voltage                       Internal

DSP Interrupt       - Ext Int4

Clock Source       - internal

 

 

Thanks a lot.

 

Alicia Corrales