Hello,
I've read every statement in this forum regarding the persistent registry on SD card. I've tried the hints from the posts and I've also read the MSDN registry based stuff again.
I also read, that Madhvi did have a solution in the past, but he did not have the source/changes now.
Its also no help, that there should be a solution in Compact 7 - our customers wants CE6 so far and mostly the next time.
I get the hive-based registry on SD to work on Atmel devices before, so I also know what to do in the past.
It would be very kind, if TI could fix this and post an overall patch or a new BSP version. I could not be the only one at this time who has this problem and like to save everything on a SD card. In all our new designs, NAND or NOR is absolutely obsolete and SD is the main memory of choice.
Would be nice if we all must not investigate more work into this as we should.
Thanks.