Part Number: AM62A7
I want to use a specific sensor on AM62A. What is the maximum camera resolution and frame rate supported by AM62A?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM62A7
I want to use a specific sensor on AM62A. What is the maximum camera resolution and frame rate supported by AM62A?
There are a few limiting factors as far as the camera resolution and frame rate are concerned:
The ISP bandwidth is usually the main limiting factor. The ISP supports up to 16-bit RAW input data. When ISP runs at maximum bandwidth with 16-bit input, the total data rate is 315MPixel/second * 16-bit/Pixel = 5Gbps. This is below the 4-lane CSI-2 Rx maximum bandwidth.
To evaluate if a camera resolution and frame rate can be supported by the AM62A, start from the simplest limiting factor: